cancel
Showing results for 
Search instead for 
Did you mean: 

What is the purpose of Carrier cancellation and Log amplifier in RF chain.

Sumeet66
Associate II

Hello ST community,

What is the purpose of Carrier cancellation circuit and Log amplifier in RF chain? We are making a standalone circuit design on our own pcb, Do we need to include that in our design?

Thanks and Regards,

Sumeet Patil

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Bart Herse
Senior II

Hi,

the carrier cancellation is used to suppress the carrier which leaks into the receiver (Self-Jammer).

It is strongly recommended to implement this part of the circuitry.

Log amplifier: If you are referring to the power detector which is connected to the 20 dB directional coupler - this could be left out, it is not necessary.

Cheers,

B

View solution in original post

4 REPLIES 4
Bart Herse
Senior II

Hi,

the carrier cancellation is used to suppress the carrier which leaks into the receiver (Self-Jammer).

It is strongly recommended to implement this part of the circuitry.

Log amplifier: If you are referring to the power detector which is connected to the 20 dB directional coupler - this could be left out, it is not necessary.

Cheers,

B

Sumeet66
Associate II

Thank you for the reply,

So, we can omit 20 dB coupler also?

Bart Herse
Senior II

​Exactly, the 20 dB Directional Coupler could be removed as well in case the power detector functionality is not implemented.

Cheers,

B

Sumeet66
Associate II

Hi Bart,

Thanks for response, I have a question what is the role of power detector? Is it used to measure receive power or transmit power?

Another question I have, we want to introduce fail safety mechanism, such as our MCU should be able to diagnose where in the RF chain there is failure?

For example, we want to check electronically whether power amplifier has failed or not? Can you give us some ideas, on how to diagnose RF chain issues.

Look forward to hearing from you.

Thanks and Regards,

Sumeet Patil