cancel
Showing results for 
Search instead for 
Did you mean: 

what configuration to be set to enter the ST25R3911B chip in low power mode & should be wakeup if RFID card is detected & give the interrupt on IRQ pin to wake up the external MCU?

RP
Associate II

In example code in library STM32CubeExpansion_NFC5_V1.3.0 for STM32L476RG-Nucleo, after pressing user BUTTON, it enters in low power mode. When it should be wake up, after again pressing user BUTTON or After detecting RFID tag? What is the program flow?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Ulysses HERNIOSUS
ST Employee

Hi,

the User button switches between using the low-power wake-up mode of the ST25R3911B and not using it.

The actually wake-up will be performed by detecting as per selected mode using capacitive plates or detuning of the LC tank (short enable of the field). Interrupt is sent to MCU which could used to wake the MCU.

Ulysses

View solution in original post

1 REPLY 1
Ulysses HERNIOSUS
ST Employee

Hi,

the User button switches between using the low-power wake-up mode of the ST25R3911B and not using it.

The actually wake-up will be performed by detecting as per selected mode using capacitive plates or detuning of the LC tank (short enable of the field). Interrupt is sent to MCU which could used to wake the MCU.

Ulysses