2024-01-11 8:59 PM
Hello!
Hope you are doing well.
I would like to check if I can get the thermal resistance Rthja and Rthjc information on Part no: M24LR04E-R.
Let me know your input and if you have any questions!
Cheers
Madhu
Solved! Go to Solution.
2024-01-12 2:02 AM
Hello,
Those values are not provided for the M24LR, but you can find them in the for the ST25DV04KC. The two devices share the same exact packages (SO8 and TSSOP8) so you can use the thermal characteristics of the SO8 and TSSOP8 of the ST25DV04KC also for the M24LR.
Best regards.
2024-01-12 2:02 AM
Hello,
Those values are not provided for the M24LR, but you can find them in the for the ST25DV04KC. The two devices share the same exact packages (SO8 and TSSOP8) so you can use the thermal characteristics of the SO8 and TSSOP8 of the ST25DV04KC also for the M24LR.
Best regards.