Skip to main content
RBhav.1
Visitor II
May 12, 2023
Solved

ST25RU3993-HPEV kit

  • May 12, 2023
  • 1 reply
  • 1047 views

I am looking to use ST25RU3993-HPEV kit for my project. Does the STM32L476RGT6 MCU (Which is included in kit), has ability to program with C language ? IOT? does the Antenna has ability to communicate with Arduino/ESP32 ? I2C/SPI?UART?

This topic has been closed for replies.
Best answer by Nick K

Hello RBhav.1,

To start developement based on the ST25RU3993-HPEV kit ST offers the schemantic of the board and the FW that is running on the board, both as open source. Please have a look at https://www.st.com/en/nfc/st25ru3993.html were all resources are available. 

Further details and resources on the STM32L476 that is used with the HPEV kit can be found at https://www.st.com/en/microcontrollers-microprocessors/stm32l4-series.html. ST also offers a set of software tools that allow to develop application for many use-cases including IOT applications written in C. 

It is also possible to use the ST25RU3993 together with other microcontrollers or system on chip solutions as ESP32. 

BR

1 reply

Nick K
Nick KBest answer
ST Employee
June 7, 2023

Hello RBhav.1,

To start developement based on the ST25RU3993-HPEV kit ST offers the schemantic of the board and the FW that is running on the board, both as open source. Please have a look at https://www.st.com/en/nfc/st25ru3993.html were all resources are available. 

Further details and resources on the STM32L476 that is used with the HPEV kit can be found at https://www.st.com/en/microcontrollers-microprocessors/stm32l4-series.html. ST also offers a set of software tools that allow to develop application for many use-cases including IOT applications written in C. 

It is also possible to use the ST25RU3993 together with other microcontrollers or system on chip solutions as ESP32. 

BR