ST25 NFC/RFID tags and readers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can I read ST25R3916 MAC address ?

I have two devices (which are with STM32F429 & ST25R 3916) from which I read NFC Wifi pairing and Bluetooth pairing tags. What can I change to make these two identical devices in terms of functionality (which are still physically different) indisting...

toshko by Associate II
  • 238 Views
  • 3 replies
  • 0 kudos

Resolved! ST25DV: why is a DC voltage delivered on VCC?

An internal voltage regulator allows the external voltage applied on VCC to supply the ST25DVxxKC, while preventing the internal power supply (rectified RF waveforms) to output a DC voltage on the VCC pin.Whats the purpose to output a DC voltage on V...

JDirk.1 by Senior
  • 222 Views
  • 1 replies
  • 0 kudos

Resolved! Integrating RFAL for ST25R3916 with STM32F2xx

I'm having trouble integrating RFAL for ST25R3916 with an STM32F2xx project. I downloaded RFAL from here: https://www.st.com/en/embedded-software/stsw-st25rfal002.html#overview. I am trying to follow the steps from section 4.3 How to Run the First Ex...

0693W00000HqoeNQAR.png 0693W00000HqoeXQAR.png 0693W00000HqohbQAB.png
PMurp.1 by Associate
  • 450 Views
  • 1 replies
  • 0 kudos

Resolved! FTM with st25r3916 without RFAL?

I would like to write my own program which can send messages and read from the mailbox on an st25dv-i2c. On one end I have a st32-L0 nucleo board which can access a x-nucleo-nfc04A1 mailbox via i2c. On the other end I have a st32-L433 connected to a ...

OSilv.1 by Associate II
  • 206 Views
  • 2 replies
  • 0 kudos

Resolved! Programming ST25TA with NFC Tap app

Dear community,for my project it is necessary to write a text on a ST25TA NFC tag and lock it afterwards permanently.For this I use the ST25 NFC Tap app (Android & iOS), but the interface is hard to understand without any guides.Is there an expert or...

0693W00000Hp6b8QAB.jpg 0693W00000Hp6b3QAB.jpg
DStei.5 by Associate II
  • 471 Views
  • 4 replies
  • 0 kudos