cancel
Showing results for 
Search instead for 
Did you mean: 

St25r95 can detect Mifare4 but no response to Mifare7 /Felica

JECKSON
Associate

Hi , we had a problem with ST25R95 NFC solution, it looks OK to detect Mifare4  card  at 10mm range, but have not any response to Mifare7 and Felica card.

this is due to NFC antenna match?

 

1 REPLY 1
Brian TIDAL
ST Employee

Hi,

do you use an ST X-NUCLEO-NFC03A1 board or a custom board? Do you use the ST RFAL library for your application or your own implementation on top of the ST25R95 commands?

Can you provide detailed information about the Mifare tag being used (mifare7 is not a known model)?

Can you provide more information about "have not any response to Mifare7 and Felica card": what is the command being used and what is the return code?

Can you connect a login analyzer on SPI (CLK/MISO/MOSI/CS) + IRQ_OUT + IRQ_IN and provide a trace of you issue?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.