cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R39R11B

J-luu
Associate II

Jluu_0-1758264667716.png

Jluu_1-1758264693204.pngJluu_2-1758264767856.pngJluu_3-1758264780780.png

 

Currently, we are developing a card reader featuring a circular NFC antenna. However, due to the lack of equipment for measuring antenna parameters, we are reliant solely on calculated theoretical values. The circuit board and antenna are depicted in Figure 1, impedance matching is shown in Figure 2, and simulation diagrams are presented in Figures 3 and 4. Is there any means to optimise the antenna design or draw the antenna? Alternatively, are any circular antennas readily available? The circular antenna requires a minimum diameter of 42mm and a maximum diameter of 50mm.

 

*This post has been translated from Chinese to comply with the ST Community guidelines.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Travis Palmer
ST Employee

Hello J-luu,

 

It is not very easily possible to tune a NFC reader without VNA.

There is a nanoVNA H4, which is quite affordable. 

Even if you use a pre-tuned 50Ohm antenna, it is recommended to check the tuning. Parasitics introduced with the layout or PCB layerstack can have very bad influence on the matching. 

One other solution is to rent a service at a university or consult an external RF design house.

BR Travis

View solution in original post

1 REPLY 1
Travis Palmer
ST Employee

Hello J-luu,

 

It is not very easily possible to tune a NFC reader without VNA.

There is a nanoVNA H4, which is quite affordable. 

Even if you use a pre-tuned 50Ohm antenna, it is recommended to check the tuning. Parasitics introduced with the layout or PCB layerstack can have very bad influence on the matching. 

One other solution is to rent a service at a university or consult an external RF design house.

BR Travis

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.