cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R3916B: Regarding the selection of an external crystal and the design of a matching circuit.

KT_25
Associate II

I have two questions.

(1) Regarding an external crystal oscillator.
For the ST25R3916B, is it necessary to have an external 27.12MHz crystal between XTI and XTO? Also, are there any points to note when selecting a crystal?

(2) Regarding the design of the antenna matching circuit.
I am trying to design a matching circuit using the NFC/RFID Calculators following the method in the AN5276 Application note. How should I decide the values ​​to enter in the "Matching inputs section" and "Inputs section" of the NFC/RFID Calculators?

1 REPLY 1
Billy OWEN
ST Employee

Hi @KT_25 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy