cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R3916 Discovery board - Unable to start USB mode.

ADant.1
Associate II

I am using ST25R3916 Discovery board to tag testing purpose and I am using ST25PC-NFC feature of discovery GUI. Even though I am able to start USB mode on Discovery board ( I can see that display on discovery board shows USB mode enabled ) but GUI does not detect the device. If i try to update the firmware it shows DFU driver issue. How can I solve this issue?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi,

there are 2 USB connectors on the Discovery motherboard:

  • J1 User USB (micro USB for connection to the PC GUI)
  • J2 STLink USB (mini USB for debug)

See figure 5 in UM2358 Getting started with ST25R3916-DISCO. Make sure to use the micro USB (User USB). Also, check the default configuration (see §4.2 in UM2358 Getting started with ST25R3916-DISCO).

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Brian TIDAL
ST Employee

Hi,

there are 2 USB connectors on the Discovery motherboard:

  • J1 User USB (micro USB for connection to the PC GUI)
  • J2 STLink USB (mini USB for debug)

See figure 5 in UM2358 Getting started with ST25R3916-DISCO. Make sure to use the micro USB (User USB). Also, check the default configuration (see §4.2 in UM2358 Getting started with ST25R3916-DISCO).

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.