cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R3911B

SONUKUMARSINGH
Associate II

Hi am using ST25R3911B DISCOVERY Board, and I am using ISO15693 Single read and write function.but this function not work properly and i found an err code after execution the code.the value not to be read and write properly. but  st25r3911WriteTestRegister(res,value);this function work properly for read and write.Do u have any suggestion regarding this .

 

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Ulysses HERNIOSUS
ST Employee

Hi,

 

well one is trying to talk to NFC tags in front of the antenna over RF and the other one just accessing registers on SPI....

 

Ulysses

SONUKUMARSINGH
Associate II
MX_GPIO_Init();
  MX_I2C1_Init();
  MX_LPUART1_UART_Init();
  MX_USART1_UART_Init();
  MX_SPI1_Init();
  MX_USB_DEVICE_Init();

  /* USER CODE BEGIN 2 */
  
  /* SPI Connection to ST25R3911 */
  spiInit(&hspi1);
  
  /* Use LPUART1 as logging UART */
  logUsartInit(&hlpuart1);
  logUsart("Welcome to DISCO-STM32L4x6\n");
  
  /* Initalize RFAL */
  rfalAnalogConfigInitialize();
  if( rfalInitialize() == ERR_NONE )
  {
      logUsart("RFAL initialization succeeded..\n");
      platformLedOn(PLATFORM_LED_FIELD_PORT, PLATFORM_LED_FIELD_PIN);
      ledOn(LED_A);
      ledOn(LED_B);
      ledOn(LED_F);
      ledOn(LED_V);
      ledOn(LED_AP2P);
  }
  else
  {
      while(1){
        platformLedToogle(PLATFORM_LED_FIELD_PORT, PLATFORM_LED_FIELD_PIN);
        ledToggle(LED_A);
        ledToggle(LED_B);
        ledToggle(LED_F);
        ledToggle(LED_V);
        ledToggle(LED_AP2P);
        HAL_Delay(40);
        logUsart("RFAL initialization failed..\n");
      }
  }

  /* For production programming: Turn ON field led, diabled by 
   * rfalSetAnalogConfig when accessing op control */
  platformLedOn(PLATFORM_LED_FIELD_PORT, PLATFORM_LED_FIELD_PIN);

  /* Initalize SW components */
  StreamDispatcherInit();
  dispatcherWorker();
if(0X00==	rfalNfcvPollerInitialize( ))
     ledToggle(LED_A);
	   else 
	  	ledToggle(LED_B);

		 

		  
		 while(1)
		 {
			 

        err = rfalNfcvPollerWriteSingleBlock(RFAL_NFCV_REQ_FLAG_DEFAULT, uid, blockNum, wrData, sizeof(wrData));
      if( err==0)
			 ledOn(LED_A);
        else	
				ledOff(LED_A);	
        err = rfalNfcvPollerReadSingleBlock(RFAL_NFCV_REQ_FLAG_DEFAULT, uid, blockNum, rxBuf, sizeof(rxBuf), &rcvLen);
        if( err==0)
				ledOn(LED_B);
        else	
				ledOff(LED_B);	
    
}
}
SONUKUMARSINGH
Associate II

I was expecting that led A and LED B ON after succesive read and write in tag. but here both led's are off.and also confused with RFAL_NFCV_REQ_FLAG_DEFAULT VALUE, is it possible to use here a particular flag value like 0x02.