2017-03-15 8:57 AM
Hello,
at the Embedded World 2017 campaign, ST25R3911B-Disco boards are given out. However looking for the software, I only found
That page only gives a data brief about installation, but no software.
Interest in those give-away gadget is highest short after aquisation by the user. So not having things ready for a beginnig user with hand-out of the gadget seems like a missed chance to me, Chances are high that many of these gadgets will end up in the drawer after the first unsuccessfully attempt to use them.
Regards
Solved! Go to Solution.
2017-03-21 6:58 AM
The PC firmware is now on line
2017-03-15 12:17 PM
here the same...
2017-03-15 3:54 PM
I've exactly the same problem. Since yesterday I'm looking for software and driver and can not find anyting.
The link STSW-ST25R001 PC software installer for ST25R3911B-DISCO in the category Tools and Software (
) refers to the page which was posted by bonnes.uwe2017-03-21 6:58 AM
The PC firmware is now on line
2017-04-14 11:46 PM
Do you also plan to release an API or software library for the board? Or could it only be used under Windows with the mentioned application?
2017-07-05 6:34 AM
Hello! I am impossible to download working PC software installer for ST25R3911B-DISCO. I download it but the archive seems broken. How can you help me, please?
2017-07-07 10:37 AM
Software downloaded from:
appears to have virus?
2017-07-07 12:30 PM
Same problem here. I really want to try this out!