Skip to main content
GDeto
Associate II
January 26, 2019
Solved

ST25R3911B and Compliance with ISO15693

  • January 26, 2019
  • 1 reply
  • 1379 views

Hello all,

I am trying to understand how to configure the  ST25R3911B to comply with the ISO15693.

In particular I do not understand how to set the Low/High Bitrate.

Looking at the datasheet of the ST25R3911B the Bit Rate Definition Register lowest achievable value is fc/128 while the ISO 15693 goes fc/2048!

I cannot find much of information how to setup the ISO15693 on the datasheet. Is there some other reference, or instructions on how to do so?

Thank you!

Update:

Checked the other questions...

https://community.st.com/s/question/0D50X00009XkWIeSAN/iso-15693-sof-eof-for-st25r3911b

https://community.st.com/s/question/0D50X00009XkWIfSAN/register-settings-for-st25r3911b-for-iso-15693

But it seems that ISO15693 is not inherently supported... So I wonder if it should be mentioned in the specs as it is more like a custom protocol implementation with coding/decoding performed in the external logic and not within the ST25 device among all.

    This topic has been closed for replies.
    Best answer by Ulysses HERNIOSUS

    Hi,

    yes the ST25R3911B does internally implement all of ISO15693-2. Bit coding/decoding and framing needs to be done in SW. ST provides software showing 1of4 high data rate using one subcarrier - e.g. inside X-CUBE-NFC5.

    Low data rate is also possible but not supported by this software. More RAM will be required and decoder logic needs to be changed.

    Regards, Ulrich

    1 reply

    Ulysses HERNIOSUS
    ST Technical Moderator
    January 28, 2019

    Hi,

    yes the ST25R3911B does internally implement all of ISO15693-2. Bit coding/decoding and framing needs to be done in SW. ST provides software showing 1of4 high data rate using one subcarrier - e.g. inside X-CUBE-NFC5.

    Low data rate is also possible but not supported by this software. More RAM will be required and decoder logic needs to be changed.

    Regards, Ulrich