cancel
Showing results for 
Search instead for 
Did you mean: 

Rewire IRQ pin in NUCLEO-NFC06A1

KVoul.1
Associate III

Hello, I accidentally connected Vcc to the interrupt pin in an X-NUCLEO-NFC06A1, now I don't get any interrupts. Is it terminally burnt or can I configure an IRQ from somewhere else on the board?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

The interrupt pin of the X-NUCLEO-NFC06A1 is connected to pin IRQ of the ST25R3916, which is an output, most likely destroyed and no chance to get the IRQ from somewhere else.

The only possibilities: replace the ST25R3916 or get a new X-NUCLEO-NFC06A1.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

The interrupt pin of the X-NUCLEO-NFC06A1 is connected to pin IRQ of the ST25R3916, which is an output, most likely destroyed and no chance to get the IRQ from somewhere else.

The only possibilities: replace the ST25R3916 or get a new X-NUCLEO-NFC06A1.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.