2020-12-23 2:43 AM
Hi,
How can I easily write/read N213 tags using rfal v2.2.0?
For the v1.3.2 version I used to call rfalISO14443ATransceiveFrame() to do it but I don't know how it's done in this latest stack version.
regards,
gaston
Solved! Go to Solution.
2020-12-23 3:46 AM
Hi Gaston,
you can use the functions in rfal_t2t.c. Depending on your needs you can also use the NDEF layer used e.g. in STSW-ST25R-LIB or X-CUBE-NFC6 to read/write NDEF on formatted tags.
Regards, Ulysses
2020-12-23 3:46 AM
Hi Gaston,
you can use the functions in rfal_t2t.c. Depending on your needs you can also use the NDEF layer used e.g. in STSW-ST25R-LIB or X-CUBE-NFC6 to read/write NDEF on formatted tags.
Regards, Ulysses
2020-12-24 2:22 AM
Thanks Ulysses, it was just what I wanted and the write / read functions work as expected.
Besides, I also have to implement a password authentication (read) access but I see in the library that it is only available for NFC-V (ISO15693) tag families. Would an implementation of a password protection be available for T2T?
regards,
gaston
2020-12-29 2:45 AM
Hi Ulysses,
Currently I see that there is no password authentication implementation in rfal_t2t. Therefore I have added my own function that works correctly and that I have no problem to share it.
/*******************************************************************************/
ReturnCode rfalT2TPollerAuth( uint32_t pwd, uint8_t* rxBuf, uint16_t rxBufLen, uint16_t *rcvLen )
{
ReturnCode ret;
rfalT2TAuthReq req;
if( (rxBuf == NULL) || (rcvLen == NULL) )
{
return ERR_PARAM;
}
req.code = (uint8_t)RFAL_T2T_CMD_PWD_AUTH;
req.pwd[0] = pwd;
req.pwd[1] = pwd>>8;
req.pwd[2] = pwd>>16;
req.pwd[3] = pwd>>24;
/* Transceive Command */
ret = rfalTransceiveBlockingTxRx( (uint8_t*)&req, sizeof(rfalT2TAuthReq), rxBuf, rxBufLen, rcvLen, RFAL_TXRX_FLAGS_DEFAULT, RFAL_FDT_POLL_READ_MAX );
/* T2T 1.0 5.2.1.7 The Reader/Writer SHALL treat a NACK in response to a READ Command as a Protocol Error */
if( (ret == ERR_INCOMPLETE_BYTE) && (*rcvLen == RFAL_T2T_ACK_NACK_LEN) && ((*rxBuf & RFAL_T2T_ACK_MASK) != RFAL_T2T_ACK) )
{
return ERR_PROTO;
}
return ret;
}You should call
rfalT2TPollerAuth(password, rfidRxBuf, 2, &rcvLen);
and expect 2 bytes of PACK in rfidRxBuf
regards,
gaston