2022-08-16 12:42 PM
I would like to be able to read the memory content from a mifare and/or Felica tag similar to how the NXP tag detector app on Android does. How would I go about doing that?
I have implemented the demo polling example using nfc03a1 and a non st chip over SPI. When reading the Felica tag I get the UID and system code but I get "check block: FAIL". it seems this if statement is failing: checkRes[RFAL_NFCF_CHECKUPDATE_RES_ST1_POS] != RFAL_NFCF_STATUS_FLAG_SUCCESS in the rfalNfcfPollerCheck function.
this is the output:
Felica/NFC-F card found. UID: 0116050028172008
>>>> 02050451100680
<<<< 0000
>>>> 090468010150
<<<< 0000
>>>> 09040A0102A1
<<<< 0000
DATA >>>> 060116050028172008010B00018001
DATA <<<<(0x800C) 0C07011605002817200801A6
00
(retCode=0)
checkres[0]:7
checkres[1]:1
checkres[2]:16
checkres[3]:5
checkres[4]:0
checkres[5]:28
checkres[6]:17
checkres[7]:20
checkres[8]:8
checkres[9]:1
checkres[10]:a6
checkres[11]:a0
ret: 5
Check Block: FAIL Data:
>>>> 02020000
<<<< 0000
>>>> 070E0A2100380118002460607C843F00
Wake Up mode startedFor the mifare tag all i get is the UID. Would using ndef commands help me read their memory content?
Solved! Go to Solution.
2022-08-22 4:33 AM
Hi,
regarding DESFire T4T formatting, see Application Note AN11004 (MIFARE DESFire as Type 4 Tag) from the manufacturer of this tag. If your application basically requires memory read/memory write only, I would suggest to use ST25TA tags instead of DESFire.for T4T and ST25TN tags instead of MIFARE UL for T2T
Rgds
BT
2022-08-17 12:35 AM
Mifare is a proprietary protocol and can therefore only be supported by its manufacturer, see e.g. also here.
For FeliCa™ see e.g. there.
Regards
/Peter
2022-08-17 1:28 AM
Hi,
Mifare: it depends, which variant: Mifare Classic is proprietary. Mifare UL / Desfire should be compatible (when formatted) to NFC Forum T2T/T4T.
This way they will be read by e.g. STSW-ST25R017 (ST25 Embedded NFC lib for ST25R95) using its ndef_rw project.
BR, Ulysses
2022-08-18 12:24 PM
Resolved the Felica memory read issue by using the correct nfcid2 and the NXP_APP defined service code in the RFAL_NFCF header file.
In terms of formating Mifare cards, what does it mean to format a Mifare Desfire to NFC Forum T4T? Is it similar to formatting a hard drive from one file system to another? Would it still be recognized as a Mifare Desfire card in the NXP Tag Info app?
Thank you,
Palden
2022-08-22 4:33 AM
Hi,
regarding DESFire T4T formatting, see Application Note AN11004 (MIFARE DESFire as Type 4 Tag) from the manufacturer of this tag. If your application basically requires memory read/memory write only, I would suggest to use ST25TA tags instead of DESFire.for T4T and ST25TN tags instead of MIFARE UL for T2T
Rgds
BT