2018-12-04 11:44 PM
Hi, i'm using NFC04A1 with NUCLEO-F401RE board, and im very new on this.
Trying to send NDEF texts (88bytes) with <1sec period ,but i cannot make it short less than 1.2sec.
Here's the while loop code with 1.2sec period.
while (1)
{
NFC04A1_LED_ON( BLUE_LED );
while( NDEF_WriteText(myMessage) != NDEF_OK );
NFC04A1_LED_OFF( BLUE_LED );
HAL_Delay(600);
HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_5);
}
I have tried many times with various HAL_Delay value and 600ms is the best for now.
Can't it be shorter?
Please give me some advices.
Thanks.
Solved! Go to Solution.
2018-12-10 1:26 AM
Hi @Patrick ,
Normally the driver is Polling the device address (I²C) to check when writing is finished. So from what I understood of your code is you are looping continuously on an I²C writing. The memory cannot be accessed in the same time by I²C and RF, there is an arbitration. That could explain why the Phone cannot access memory except if you give time to do (HAL_Delay).
I think you should reconsider your sequence and only write in I²C only when it is needed to allow time for the RF commands.
May I also suggest you to have a look to the Datasheet of the ST25DV (https://www.st.com/content/st_com/en/products/nfc/st25-nfc-rfid-tags-readers/st25-dynamic-nfc-tags/st25dv-i2c-series-dynamic-nfc-tags/st25dv04k.html), this device has some features that could help to better manage arbitration between I²C and RF (e.g. GPO, ...).
Hope this can help.
Regards.
2018-12-06 2:11 AM
Hi @Patrick ,
When you write data to the tag the driver is polling the device on I²C to know when it has finished writing. So normally, you shouldn't have to use HAL_Delay to wait until data are written to memory.
Writing 4 bytes takes about 5 ms max for this memory, so 88 bytes should take about 110ms + MCU processing and I²C time.
What is the problem removing the HAL_Delay in the loop?
Regards.
2018-12-09 3:57 PM
Hi Rene, Thanks for the answer.
If i delete HAL_Delay in the loop, NDEF Message cannot be received.
Receiver (Phone) does not respond or find a tag without any messages inside(Empty Tag detect).
If so, what do you think i should do to get the messages with period under 1 sec??
Waiting for your answer.
Thanks.
2018-12-10 1:26 AM
Hi @Patrick ,
Normally the driver is Polling the device address (I²C) to check when writing is finished. So from what I understood of your code is you are looping continuously on an I²C writing. The memory cannot be accessed in the same time by I²C and RF, there is an arbitration. That could explain why the Phone cannot access memory except if you give time to do (HAL_Delay).
I think you should reconsider your sequence and only write in I²C only when it is needed to allow time for the RF commands.
May I also suggest you to have a look to the Datasheet of the ST25DV (https://www.st.com/content/st_com/en/products/nfc/st25-nfc-rfid-tags-readers/st25-dynamic-nfc-tags/st25dv-i2c-series-dynamic-nfc-tags/st25dv04k.html), this device has some features that could help to better manage arbitration between I²C and RF (e.g. GPO, ...).
Hope this can help.
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.