2022-09-12 1:27 AM
Hi Experts
I used NFC Tap App to transmit data(use FTM write message cmd), transmit 10 byte
As my analysis below the last 4 byte should be the CRC(4 byte),I think it's use CRC32 method, but I can't calculate the result as same as the App
Results by using on-line CRC calculator
Could you please verify this for me? thank you very much!
Solved! Go to Solution.
2022-11-08 3:25 AM
Hi,
The ST25SDK contains a class for this CRC verification. You can use it with:
import com.st.st25sdk.Crc;
byte[] computedCrc = Crc.computeCrc(data);Best regards
Olivier
2022-09-12 2:14 AM
Hello Jerry,
I think you are mixing the Write message command (ISO15693 frame) with something else.
The Write Msg command format is:
02 aa 02 | 0f | 05 00 01 02 03 04 05 06 07 08
cmd code | msg len | data
Control Byte and Packet length and CRC32 you are inserting in the middle of the Write Msg command do not belong to this command.
Best regards.
2022-09-13 9:47 AM
Hi, can you provide a cite to the document with the CRC and example packet code, and perhaps the ISO standard that's coming from.
Thanks,
2022-09-27 2:53 AM
Hi Jerry,
Any news from your side on this issue ?
Best regards.
2022-10-02 7:26 PM
Hi, Sorry for lately respond because I just ignore the CRC and proceed to develop my application.
The protocol I described is "FTM protocol" which you can refer to below url:
And I just wanna find which CRC32 method was adapted in ST FTM protocol
Thank you!
2022-11-08 3:25 AM
Hi,
The ST25SDK contains a class for this CRC verification. You can use it with:
import com.st.st25sdk.Crc;
byte[] computedCrc = Crc.computeCrc(data);Best regards
Olivier