cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple tags ID in the GUI with the Inventroy button. Why is that?

CMath
Associate

Hello

I made some tests with the eval board. I use the ISO15693 standard to read some tags. I wanted to read up to 20 tags. Very often I get same tag ID twice in one reads cycle. Is this normal? I had the problem in the GUI over the inventory button.

Regards

Céline

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Ulysses HERNIOSUS
ST Employee

Hi Celine,

I found this request in the basement - seems to have escaped our radar.

In case this is still valid open, then you will need to share more details on your setup: Which board, which version of software, which functions did you used and also the kind of tags would be important.

Regards, Ulysses