cancel
Showing results for 
Search instead for 
Did you mean: 

IOS NFC restartpolling

denma0513
Associate II

Hi

I`m going to develop a app to display image on ePaper by coreNFC ISO15693, but i have only 20sec to transmit data and display image when phone connect on epaper .  

I can use session.repolling() to extend life scycle of NFC session lower iphone13 or below, but else version (iphone15, iphone16) is not working .

As far as I know, i have 60sec to trans data when i to begin a new NFCTagReaderSession, but actullary i have only 20sec. 

If I need more time to transmit, what solution i can do?

 

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi denma0513,

It would seem that since iPhone15, Apple closed possibility to extend the sessions beyond the allowed amount by "renewing" them.

I encourage you to have a look into the apple forum thread "https://developer.apple.com/forums/thread/765747"

For the time being, I don't have any idea/solution on how extending iOS CoreNFC life cycle over 20s, as it depends on system itself, and we don't have any control on it. 

We could use the apple feedback assistant for refining the feature. ref to  Bug Reporting - Apple Developer 

sorry again for not being able to help you more.

 

 

View solution in original post

4 REPLIES 4
victor laraison
ST Employee

hi Demna0513,

Currently there are two NFC timeouts we are not able to influence because there is no API.

  • A NFC Session has a maximum lifetime of 60 seconds, independent from any card communication.
  • When a card was detected the connection will only last for 20 seconds.

Combined there is also something like a worst case:

  • The user presents the card 55 seconds after the session was started: The connection will only last for the remaining 5 seconds of the session.

Normally, whatever is iphone model, behavior should be same on every iphone. 
Please, Could you check iOS version used ? 

I tried with iphone15 pro + iOS 17.4, and behavior is as described above.

hope it helps.

br,

 

Hi

 

there is following is my test result, use session.restartpolling() to extend the NFC session life scycle.

iphone Xs (IOS 17) : OK 

iphone Xs (IOS 18.0.1) : OK 

iphone 12 pro (IOS 17.4.1) : OK 

iphone 13 (IOS 17) : OK 

iphone 15 (IOS 17) : fail

iphone 15 (IOS 18) : fail

iphone 16 (IOS 18) : fail

denma0513
Associate II

Hi

So I have no any soluction to extend the life cycle, if I need over 20 second to done my task?

Hi denma0513,

It would seem that since iPhone15, Apple closed possibility to extend the sessions beyond the allowed amount by "renewing" them.

I encourage you to have a look into the apple forum thread "https://developer.apple.com/forums/thread/765747"

For the time being, I don't have any idea/solution on how extending iOS CoreNFC life cycle over 20s, as it depends on system itself, and we don't have any control on it. 

We could use the apple feedback assistant for refining the feature. ref to  Bug Reporting - Apple Developer 

sorry again for not being able to help you more.

 

 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.