2021-10-13 8:40 AM
I'm trying to read a T2T tag with NFC card reader, Nucleo expasion board attached to STM32F103 Nucleo board. I'm using an example from X-CubeExpansion_NFC3
This tag is well formatted with NDEF, but when I try to read with this example, I get an error in ndefPollerNdefDetect(). This funtion returns ERR_PROTO.
If I read this tag with any other application, I can read it content.
Can you help me with this problem. I'm sure, I'm doing something wrong, but I don't know what is
Thank you in advance, looking forward to hearing from you
Carmen
Solved! Go to Solution.
2021-10-14 11:41 PM
Hello Ulysses,
I will take your advice into account and buy the NFC tags from the forum.
Thank you very much for your help
Best Regards
Carmen
2021-10-15 12:07 AM
Hello again,
My customer wants to use Mifare Ultralight, or Mifare Ultralight C. Are these tags compatible with the ST25R95 RFAL and NDEF libraries?
Thank you
Best regards
Carmen
2021-10-15 1:02 AM
Hi Carmen,
those 2 models can be configured as NFC Forum Type 2 tags. Once configured as NFC Forum Type 2 tags, they are compatible with the ST25R NDEF library. Make sure to check with the tag manufacturer for the proper tag configuration.
I would recommend to base your application on latest RFAL and NDEF from the ST25 Embedded NFC library that provides full support of the memory lock TLV and reserved area TLV that may be used with some NFC Forum Type 2 tags.
Please not that ST25TN tags are NFC Forum Type 2 tags and are ready to use.
Rgds
BT