2024-03-23 03:21 AM
I have purchased X-NUCLEO-NFC03A1 (CR95HF) evalboard, and nucelo-F072RB board.
I want to develop RFID reader/writer . Please suggest a firmware example code which I can program in the eval board. Secondly Does ST has any PC based utility which can be used to send commands to nuclo board to read and write RFID cards/tags. Please share videos which demonstrate the same.
Thanks
Solved! Go to Solution.
2024-03-25 01:33 AM
Hi,
The ST25 embedded NFC library (STSW-ST25R017) provides FW support for the X-NUCLEO-NFC03A1 expansion board. It contains various ready to use examples (such as simple polling, NDEF read/write, etc.) running on NUCLEO-L476RG. This can be easily ported on NUCLEO-F072RB.
The FW is running in standalone mode on the micro controller so there is no PC based utility for the nucleo board.
Rgds
BT
2024-03-25 01:33 AM
Hi,
The ST25 embedded NFC library (STSW-ST25R017) provides FW support for the X-NUCLEO-NFC03A1 expansion board. It contains various ready to use examples (such as simple polling, NDEF read/write, etc.) running on NUCLEO-L476RG. This can be easily ported on NUCLEO-F072RB.
The FW is running in standalone mode on the micro controller so there is no PC based utility for the nucleo board.
Rgds
BT
2024-03-25 03:12 AM
Hi Brian,
Thanks for the input, Please suggest porting steps.
2024-03-25 05:41 AM
Hi,
the most simple is to generate your project from STM32CubeMX. See https://community.st.com/t5/st25-nfc-rfid-tags-and-readers/hello-i-have-a-question-that-x-nucleo-nfc03a1-cann-t-read-and/td-p/273839 that contains an example of X-NUCLEO-NFC03A1 ioc file for NUCLEO-L476RG that can help for configuring NUCLEO-F072RB (SPI,LEDs, log UART, etc.). For the SPI, make sure to use the proper prescaler according to your clock settings. Check as well the proper pin assignment.
Rgds
BT