2020-09-28 10:36 PM
i am trying to write data using i2cset function of linux but when i write 00 value to 0x01 and read same addreess it returns me 00 value.
root@var-som-mx6:~# i2cset -y 2 0x53 0x00 0x01
root@var-som-mx6:~# i2cdump -f -y 2 0x53
No size specified (using byte-data access)
0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef
00: 00 00 ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
10: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
20: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
30: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
40: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
50: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
60: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
70: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
80: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
90: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
a0: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
b0: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
c0: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
d0: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
e0: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
f0: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ................
root@var-som-mx6:~#
Solved! Go to Solution.
2020-09-30 4:23 AM
Hello Mpraj.19,
From my understanding, you cannot use i2cset and i2cdump to consistently access the ST25DV-I2C memory, because this device requires 2 bytes for internal address (while these commands only accept 1 byte of register address).
Maybe the first byte written of i2cset could be used as the 2nd addressing byte, but this trick cannot work for the i2cdump.
Also, the ST25DV-I2C as an internal address counter and when you do an "i2cdump -f -y 2 0x53" you're actually reading from this internal address counter (and not from offset 0).
Please note as well that after a write the internal address counter poinst to the next address after the one that was written.
However I'm pleased to let you know that we just released the STSW-ST25DV007 software package providing a Linux user space driver for the ST25DV-I2C, available here:
This software package comes with a User Manual for easy ramp-up.
Regards
2020-09-29 3:09 AM
Hello,
Please be aware that memory addresses are coded on 2 bytes in the ST25DV04K. You may try 0x53 0x00 0x00 0x01 (the 0x00 0x00 are the memory address pointer and 0x01 is the data to be written).
Best regards.
2020-09-30 4:23 AM
Hello Mpraj.19,
From my understanding, you cannot use i2cset and i2cdump to consistently access the ST25DV-I2C memory, because this device requires 2 bytes for internal address (while these commands only accept 1 byte of register address).
Maybe the first byte written of i2cset could be used as the 2nd addressing byte, but this trick cannot work for the i2cdump.
Also, the ST25DV-I2C as an internal address counter and when you do an "i2cdump -f -y 2 0x53" you're actually reading from this internal address counter (and not from offset 0).
Please note as well that after a write the internal address counter poinst to the next address after the one that was written.
However I'm pleased to let you know that we just released the STSW-ST25DV007 software package providing a Linux user space driver for the ST25DV-I2C, available here:
This software package comes with a User Manual for easy ramp-up.
Regards