2023-10-11 11:44 PM
我有一个能源供应项目,并购买了X-NUCLEO-NFC07A1和NUCLEO-STM32L476RG。但是,我在EN中使用了EH代码。X-Cub-NFC7,现在我想根据此代码降低能耗。我应该如何编辑代码,使STM32L4具有最低的功耗并且只能完成LED闪烁测试?
Solved! Go to Solution.
2024-02-01 4:00 AM
please refer to the datasheet of STM32L476 to see how you can program it in low power mode.
2023-10-11 11:45 PM
I have an energy supply project and purchased X-NUCLEO-NFC07A1 and NUCLEO-STM32L476RG. However, I used the EH code in EN. X-Cub-NFC7, now I want to reduce energy consumption based on this code. How should I edit the code so that the STM32L4 has the lowest power consumption and can only complete the LED flicker test?
2024-02-01 4:00 AM
please refer to the datasheet of STM32L476 to see how you can program it in low power mode.