cancel
Showing results for 
Search instead for 
Did you mean: 

CR95HF UART Speed Change

LM
Associate II
Posted on March 22, 2018 at 19:38

I'm Using the CR95HH under a linux Microcontroler.

in this case, I'm using the UART port to communicate (not SPI), the default BaudRate is 57600, and works fine, but when I try to change the Baud rate to maximum Speed (Datasheet mention 2 Mbps max), I can't find the right procedure to do that.

the page 38 of

Data

sheet

have the description of command 0x0A,  according with this, we need to use a formula to calculate the BaudRate ==> '13.56 /(2*<BaudRate>+2) Mbps', where 'BaudRate' is any number from 0 ~ 255.

If I apply this formula, no one number give me the exact Baudrate than Linux support. in any case, I use the most closer to linux Standard. but the only one than works is the Default (B57600)

By the Way, I'm using 'C' under linux

my Actual procedure is:

1.- Open Uart port at 57600

2.- Send WakeUp command to Device

3.- send new Baudrate command (0x0A 0x01 0x05)  ==> 0x05 for 1.13 Mbps (Linux more closer B1152000)

4.- Close Uart Port

5.- Open UART at 1152000

6.- Start Using...

I try many different speeds but the only one than works is the default.

any Idea?

the Linux UART BAUD supported are (from termios.h):

=================

.

.

.

#define B57600 0010001

#define B115200 0010002

#define B230400 0010003

#define B460800 0010004

#define B500000 0010005

#define B576000 0010006

#define B921600 0010007

#define B1000000 0010010

#define B1152000 0010011

#define B1500000 0010012

#define B2000000 0010013

#define B2500000 0010014

#define B3000000 0010015

#define B3500000 0010016

#define B4000000 0010017

=======================

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on April 03, 2018 at 16:17

Hi Luis,

If you are using the ST25DV64K please refer to the chip datasheet in order to check the commands supported at 53kbps.

http://www.st.com/resource/en/datasheet/st25dv64k.pdf

Using the CR95HF you will  have to switch the speed via the protocol select command just before executing your Fast command. then go back to the standard speed.

Regards

PYB

View solution in original post

3 REPLIES 3
Posted on March 27, 2018 at 17:12

Hello Luis,

Using a MB1054B RF transceiver demonstration board from ST with a CR95HF configured with UART  means setting the SS10 and SS11 input pins to 00  and the STm32 USART communication configured I have reproduce your sequence described above.

All was working from default value 57600 up to 2.26Mbps

I have checked the timings with an oscilloscope and 2 probes connected to TX part provided by the STm32 and RX feedbacks provided by the CR95HF.

With the sample I have,  here are the following measurements done on an echo command after the UART baud rate setting.

 

Loaded   Valuefreq calculatedfreq expected Linux baud  rateTX 8bits (us) from STM32RX 8 bits (us ) from CR95HFTX rate measured (bps)RX rate measured (bps)delta RX/Baud rate linux%

316950001500000 4.719417142851695131195130.70.130087

5113000011520007.117.07011125176113152620474.280.017773

6968571.4310000008.2218.2545973117.6969168.330831.670.030832

B56500057600014.21714.1243562706.6566399.89600.2490.016667

D484285.7150000016.44116.5128486588.4484472.715527.350.031055

E45200046080017.77517.7086450070.3451757.99042.0970.019623

1C233793.123040034.23234.1663233699.5234148.93748.8540.016271

3A114915.2511520069.55169.5833115023.5114970.1229.8850.001996

7557457.62757600139.009139.17657550.2357481.17118.82510.002063

I suggest you to execute your sequence and measure on RX and TX line the data rate when executing  an echo command after programming the UART speed. Try with 3A and 05 it seems to be the closest of the LINUX values. 

Hope it will help

Regards

PB

Posted on April 02, 2018 at 20:01

Hi Peter

I have working the NFC 

CR95HF UART at 1Mbps, that is enough for now. Thank you.

Now I need the data rate speed from CR95HF and TAG (NFC/RFID ST25DV64K)

At this time the I have communication @ 26Kbps, but we need 53 kbps (Supports the 53 kbit/s data rate with

Fast commands).

when I select that speed sending Select Protocol command (section 5.4 'Protocol Select command (0x02) description')

>>>0x02020115 

<<<0x0000

after send this command and receive (accept command), I'm loosing the communication with TAG,

it is any other command to enable this 53Kbps speed at TAG or NFC reader?

Thank you

Posted on April 03, 2018 at 16:17

Hi Luis,

If you are using the ST25DV64K please refer to the chip datasheet in order to check the commands supported at 53kbps.

http://www.st.com/resource/en/datasheet/st25dv64k.pdf

Using the CR95HF you will  have to switch the speed via the protocol select command just before executing your Fast command. then go back to the standard speed.

Regards

PYB