Skip to main content
VSoni.1
Associate II
September 30, 2021
Solved

Cannot find firmware update file for ST25R3916 - DISCO Board

  • September 30, 2021
  • 2 replies
  • 940 views

Hey, I recently ordered an ST25R3916-DISCO board for communicating with ST25 RFID tag antennas. I connected the board to my PC via the micro-USB cable and was able to detect my antenna via the R/W feature on the MCU. Furthermore, I downloaded the ST25R3916 discovery GUI software on my PC to obtain the RFID communication data (specifically RSSI values) on the computer. However, the software UI is grayed out and is not recognizing my board. I looked up the user manual for setting up the ST25R3916-DISCO board and it specifies installing the "DISCO_STM32L4x6.hex" firmware file. However, I am not able to locate the file in the installation directory. The file that I have in the firmware directory is "ST25R3916Demo_MB1414B_v1.2.0.hex". I also downloaded the "STSW-ST25R011" file which is the firmware for the ST25R3916-DISCO board, but couldn't locate the firmware file in there as well. Please let me know how I can get the discovery GUI to identify my board.

    This topic has been closed for replies.
    Best answer by VSoni.1

    Okay, I set the DISCO board in USB mode and was able to upgrade the firmware. I also am able to detect the RFID tag with an antenna using the ST25PC-NFC.

    2 replies

    VSoni.1
    VSoni.1Author
    Associate II
    September 30, 2021

    Okay, so I tried installing the MB1414B firmware update in the Discovery GUI software, and this is the error I received:

    "Potentially the STM32 Bootloader driver was not properly installed. Please install the driver from the Generic Discovery GUI installation directory using the device manager. Then try again."

    How do I go ahead with this? I notice that there are some driver files located under STMicroelectronics/ST25R3916_Discovery_GUI/Tools/STM32CubeProgrammer. I have 64-bit Windows 10 software; so which driver would be appropriate for me? Also, when I connect the DISCO board using the micro USB, I don't see an additional device pop up in my device manager.

    VSoni.1
    VSoni.1AuthorBest answer
    Associate II
    September 30, 2021

    Okay, I set the DISCO board in USB mode and was able to upgrade the firmware. I also am able to detect the RFID tag with an antenna using the ST25PC-NFC.