ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How can we read/write using SPI

Hi,I don't really understand the datasheet of the ST25R3916 IC chip.At page 53, they show an exemple of a direct write command. As I understand, we need to send 1-1-C5-C4-C3-C2-C1-C0. When I check table 13 to see the command code that go for bits C5....

ANaud.1 by Associate II
  • 4465 Views
  • 20 replies
  • 0 kudos

Resolved! SPI interface for STM32L476VG

STM32L476VG is the MCU we are interfacing with ST25R3911B using SPI.what we have understood from some search is that we need RFAL (abstraction layer) to interface with RF HAL.Then once we integrate RFAL and RF HAL in our system workbench(ac6) project...

RShiv.1 by Senior
  • 55107 Views
  • 190 replies
  • 0 kudos

Resolved! ST25R3911B Collision Resolution returns TIMEOUT_ERR

Hi,I have ported RFAL library to ESP32 platform and have set up proper interrupts for it to function in capacitive wakeup mode.So the issue:We are using RFAL-HL ( higher layer ) in our project ( based on X-Cube-NFC5, but using the latest version of R...

0693W00000AMH8GQAX.png
AShar.10 by Associate II
  • 1824 Views
  • 9 replies
  • 0 kudos

Resolved! RSSI Measurement via ST NFC Sensor App

Hello,I am a newbie to the field of RF communication. I am planning to design an antenna using the ST25TV IC. Ultimately, I want to measure the Received Signal Strength Indicator (RSSI) value of the RF communication. I am thinking of using the ST NFC...

VSoni.1 by Associate III
  • 1170 Views
  • 1 replies
  • 0 kudos