2026-04-22 10:47 PM - last edited on 2026-04-28 2:54 AM by Andrew Neil
Hi,
I am presently planning to use Viper265K part for High Voltage Buck converter design with below requirements:
| Min | Max | |||
| Vin | 200 | 900 | V | |
| Vout | 4.5 | V | +/-5% | |
| Iout | 0.44 | A | ||
| Pout | 2 | W |
With above requirements the duty cycle for the device is observed to be 0.5%. Please can you
help me to know if the device can be used for such low duty cycle and what would be recommendation from your side
for achieving above design requirement.
2026-04-28 3:01 AM
Hi Peter,
Thank you for your support and reply to the queries in the thread I will try to make a tradeoff on either load or input voltage for the Buck so that the Viper267K can be utilized.
Thanks again.
Regards,
Shrikant Bhairavkar