cancel
Showing results for 
Search instead for 
Did you mean: 

using ST7 Toolset Devel. tool Visual developer for ST72141 vrs ST72MC.

gclink
Associate
Posted on May 30, 2005 at 14:32

using ST7 Toolset Devel. tool Visual developer for ST72141 vrs ST72MC.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
gclink
Associate
Posted on May 17, 2011 at 10:18

Is is possible to convert a project created under the older ST7MTC2 Configuration/Programmer programs ( ie via the *.mtc intermediary file) to the newer ST7 Toolset Devel. tool St7 Visual developer, ie are the old 8 bit assember and linkers there, and can the project files be imported or rebuilt, and if so how?

Also, the excel spread sheet for 8 pole motors is corrupt on my CD, is this file available on your website, and can it generate all the timer values and ration that the Configuration program does ( ie essentially create the mtc file?)

jean-marie
Associate II
Posted on May 17, 2011 at 10:18

I send to you the zip file with source and project workspace allowing to assemble soft for ST72141 running on the Kanda kit Hardware. You have to know that this software is running using the SPI communication. Data of the *.mtc file are the one corresponding to dep_prep.txt anddeframp.txt of the project.

I attached a corrected spd82.xls files allowing you to generate the acceleration ramp and to set the speed parameter.