cancel
Showing results for 
Search instead for 
Did you mean: 

Universal Motor Control

jrsenent
Associate
Posted on March 01, 2004 at 05:03

Universal Motor Control

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
jrsenent
Associate
Posted on May 17, 2011 at 10:17

Hi.I've been asked to control the speed of a universal motor and I don't really know what microcontroller I should use.It would be very useful if you could give me some tips on this issue.

Thank you so much guys.
gaetano
Associate II
Posted on May 17, 2011 at 10:17

Hi,

I think that you intend to use an angle parzialization phase strategy to modulate the power into the motor.

If yes, what you need is a general purpose 8-bit micro with the following caracteristics:

- one timer to read the speed of the motor by a sensor;

- one timer to turn on the triac properly during one 50/60 Hz mains cycle;

- A/D converter to fix some ext parameters (reference speed, etc.)

There exists a micro , the ST52440, that owns a peripheral managing directly the driving of a triac in phase parzialization.

The Application Notes 'AN1607' e 'AN1221' should help you to develop your control.

Regards,

tanio