cancel
Showing results for 
Search instead for 
Did you mean: 

STMP34 Energymeter IC Analog pin maximal Input current.

YCai.2
Associate

Hello, Could any body tell me the maximum input current of Analog pin (VIP, VIN, IIP, IIN)? From the datasheet i can only find the maximal analog pin Input voltage with -0.7 to 0.7V.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @YCai.2​, to the community!

Due to the high input impedance of 8Mohms, these analog inputs should never have any significant current flowing into them.

Do you need this parameter to protect the device?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.