cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP1 not recovering on variable power SUPPLY, start from 0v to and rise to 5V and vice versa.

Ara.1
Senior

STPMIC1APQR is a PMIC, how to recover from lock state, as the STM32MP1 RTSn pin is not going to HIGH , 

and this situation on power variable supply decrease down to 1 v and then back to 5 v

1. no log is observed on console during not power up variable supply.

2. but if i unplug and insert the 5v preset power supply  , then unit boots up.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @Ara.1​ ,

Looks like this post address similar question than https://community.st.com/s/question/0D53W00000sAojxSAC/stpmic1-enter-to-unknown-state-when-the-board-is-powered-with-a-specific-ramp-and-is-unable-to-power-up ? Right ?

Please, provide what @PatrickF​  request :

in order to help @Vincenzo​, could you provide:

  • the STPMIC1 version (visible on UART console in very first lines of TF-A log during boot)
  • plot 24V, VIN (5V), BUCK3 (VDD) and RSTn curves in case of 'slow ramp up' failure

Regards.

Thanks,

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.