STEVAL-SPIN3201 and MATLAB/SIMULINK
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-10-10 2:10 AM
Hi,
[1] Is this board supported for automatic code generation in MATLAB/SIMULINK ?
[2] How high must the electrical rotary field resolution be for FOC operation, if I want to operate the PMSM without an observer?
[3] Is it possible to switch the operating mode BLDC (Hall sensors or BEMF) and FOC (encoder or observer) without board configuration ? Or do I generally have to change the firmware and hardware of the board like X_NUCLEO-IHM08M1 ?
Best Regards
Aaron
- Labels:
-
Motor Control Hardware
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-12-07 8:33 AM
Hi, im back with new knowledge.
I write here, so that in the future the question is answered.
[1] Yes with MAT/TARGET, but if is possible, write everything in C code !
[2] This is still an open question I can not answer until the middle of 2020, but 1 degree electrical resolution is definitely a good value.
Depending on the number of pole pairs of the motor you have to convert this, for your mechanically Encoder.
[3] Yes, I think this is with a SyncFlag possible, but first I must try it.
If you want to drive your motor with an encoder and hall sensor, you must create a new pcb with the same circuit. And do not forget to config you cubeMX icon file for this feature ;)