cancel
Showing results for 
Search instead for 
Did you mean: 

Would like to use STNRGPF01 Digital Controller for a system with 480 VAC input. The AC input voltage sensing is isolated, is there a reason this can't be used at 480 VAC?

DCook.2270
Associate

When trying to set up a simulation in E-Design, the highest input voltage that can be input is 265?

If this can be used at 480 VAC as I suspect, how do I get the voltage settings on the E-desgn tool revised

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0