cancel
Showing results for 
Search instead for 
Did you mean: 

Used eDesignSuite to design an isolated AC to DC Flyback converter circuit for wide voltage AC input, and 5V, 0.8A DC output.

Not applicable

The eDesignSuite result and my schematic are attached.

A PCB was manufactured as per the eDesignSuite BOM and design guidelines.

I connected mains to the circuit without SJ4 being bridged. Rin immediately blew. The design BOM specified a 7.5Ω , 2W resistor. Guessing that inrush current may be larger due to my using 4.7uF instead of 4.3uF at CIN1 and CIN2 , I replace the resistor with a 6.8Ω , 4W, and this worked.

The no-load voltage measured at TP8 was 5.8V.

When I connected a 47Ω , 5W resistor between TP8 and GND, the voltage at TP8 dropped to about 0.9V.

Any suggestions regarding my approach towards finding out what I might do to find a possible problem will be greatly appreciated.

Thank you.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0