cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-CTM011V1A

PGinhson
Associate III

Hi, I'm new with STM microcontrollers. I have several years programming Microchip PIC and develops with this other brand.

I want to start a project with this Brand STM, then I bought a Nucleo F411. With this one I tried some examples an all worked fine. Then I bought an STEVAL-CTM011V1A and STEVAL-CTM012V1A to evaluete the Motor Control, I need to decide Driver, Controller, Power, etc.

With this board I purchased the suggested STLINK-V3 programmer with the isolator accessory. Could someone help me explain how I program the STEVAL board with the STLINK? There isn't much explanation for that, I've been searching and can't find an answer.

While I have experience programming other things, I can't figure this out.

I would appreciate the help.
Greetings.

Blessings on your courage, that's the way to the stars
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Andrew Neil
Super User

@PGinhson wrote:

Could someone help me explain how I program the STEVAL board with the STLINK? .


You connect the ST-Link to the SWD connector on the board - see Fig 2 in the User Manual.

You can download documentation & other support resources - including the User Manual - from the Product Page:

https://www.st.com/en/evaluation-tools/steval-ctm011v1.html#documentation

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

View solution in original post

3 REPLIES 3
Andrew Neil
Super User

@PGinhson wrote:

Could someone help me explain how I program the STEVAL board with the STLINK? .


You connect the ST-Link to the SWD connector on the board - see Fig 2 in the User Manual.

You can download documentation & other support resources - including the User Manual - from the Product Page:

https://www.st.com/en/evaluation-tools/steval-ctm011v1.html#documentation

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi.
Thank you, but the SWD connector un the STLINK is not compatible with the SWD connector on the board.
The STLINK came with several flat cables and a colorfull cables for other connector (CN9).
I don't understand why the connectors on the programmer and the STEVAL board are not compatible. Do I have to make a special cable to connect the STD14 of the STLINK with the SWD of the STEVAL?

Blessings on your courage, that's the way to the stars

@PGinhson wrote:

I don't understand why the connectors on the programmer and the STEVAL board are not compatible. ?


It does seem pretty dumb - especially as the standard debug connectors for ARM chips are so well established!

:face_with_rolling_eyes:

 


@PGinhson wrote:

 Do I have to make a special cable to connect the STD14 of the STLINK with the SWD of the STEVAL?


Yes.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.