cancel
Showing results for 
Search instead for 
Did you mean: 

STC3115 Adjusting Configuration

Chip Weller
Associate
Posted on January 30, 2018 at 00:22

After reading the STC3115 datasheet (D023755 Rev 8) and system integration (AN4324), plus FAQ and the driver code on GitHub, I have questions about the REG_VM_CFG, REG_CC_CFG, REG_VM_ADJ and REG_CC_ADJ.

Are the *_CFG parameters automatically updated by the IC?

If not, is there an algorithm I should used to adjust them with the *_ADJ registers?

Thanks

#stc3115
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0