cancel
Showing results for 
Search instead for 
Did you mean: 

Remnants of stall detection in L6472 and L6482 datasheets

Blacbird
Associate II
Posted on August 21, 2017 at 12:34

Hiho,

there are still remaining hints of stall/step loss detection (for example at the description of the FLAG pin) in the datasheets of the above mentioned ICs although they are only implemented in the L6480/L6470. That way we only realized that these features are not implemented after we were quite far into a project. Would it be possible to remove those references to avoid misunderstandings like this in the future?

Cheers,

Tobias of Blacbird Technologies

#stepper-driver
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Enrico Poli
ST Employee
Posted on August 24, 2017 at 16:08

I'm sorry the error in the documentation led to this misunderstanding.

In the latest

http://www.st.com/content/ccc/resource/technical/document/datasheet/1e/f1/a3/3f/3e/49/44/02/DM00047136.pdf/files/DM00047136.pdf/jcr:content/translations/en.DM00047136.pdf

 published on our website (Rev 5) I found no references to the stall detection feature.

In the

http://www.st.com/content/ccc/resource/technical/document/datasheet/08/7b/6c/c9/3f/a5/43/7d/DM00067131.pdf/files/DM00067131.pdf/jcr:content/translations/en.DM00067131.pdf

one (Rev 6) there are still some references in the paragraphs dedicated to the blanking. They will be corrected in the next revision.

Thanks for your feedback

Posted on August 29, 2017 at 16:24

Thanks for caring about this issue. In rev5 of the L6472 datasheet step loss is still mentioned as an alarm condition for the flag pin on page 18, but you are right, this should not lead to any misunderstanding.

Posted on August 31, 2017 at 10:00

Thanks, I'll add the error in L6472 datasheet - page 18 in the correction list.