Motor Control SDK5.2 with STM32F429ZI
I attended the excellent motor control sessions last week at the ST Developers Conference in Santa Clara, CA. At the presentation I received the Nucleo F302R8 and X-Nucleo-IHM07M1 boards which I've been experimenting with. However, I would now like to use ST Motor Control Workbench to target the STM32F429ZI chip we are looking to use in our custom motor control systems. To get started, I would like to pair the X-Nucleo-IHM07M1 with the Nucleo F429ZI development board, but I don't see a way of selecting the STM32F429ZI MCU in the Motor Control Workbench.
The closest I can get is in the "MCU and Clock Frequency Selection" is choosing "STM32F4xx" as the MCU type and "STM32F417IG" as the MCU. With this I can produce the ST32CubeMX project, but within STM32CubMX, I can't change the MCU to the actual STM32F429 MCU I would like to target.
Is there a way of using the ST Motor Control Workbench to easily target the STM32F429? Is there an alternative way of using the STM32CubeMX to manually configure a project with the Motor Control middleware and the STM32F429 MCU?
Thanks,
Mike Thompson