L6235 commutation scheme
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-31 1:34 AM
We got a problem with a specific motor:
With the standard connection one direction of rotation has a significant lower torque and also at 2 specific hall sensor states the current to the coil is switched off !
Changing the connection of the motor coils and Hall sensors ( OUT1-> coil2, OUT2->coil3, OUT3-> coil1 and the hall connections the same) cures the problem.
What is the reason for that ?
There is no hint in the data sheet, no hint in an application note. Also when i tried to get in contact with ST i failed.
ST seems to have the philosophy 'our products, your problem' To get in contact with a FAE is impossible whether trying via distributors or even with a desperate call to ST headquarter here in Germany.
I regret very much to use a Product from ST because if there is an (even serious) problem one ist left alone!
Worst support ever !
#l6235- Labels:
-
Motor Control Hardware
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-02-01 5:32 AM
I'm sorry for your bad experience with our customer support.
For sure this is not the message we want to give to our customer.
Going back to your issue.
Could you share the datasheet of the motor and some waveform about the anomalous behavior you obtain with the other configuration? (OUT1-coil1, OUT2-coil2, OUT3-coil3 and the same for the hall sensors, I guess).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-02-01 8:31 AM
Hello Enrico,
very nice to get in contact with a real person at ST.
We are using an EC13 Motor from Maxon (430155). We also tried out different other motors from Maxon, they are all working.
Connecting the EC13 motor in the normal scheme (OUT1-coil1, OUT2-coil2, OUT3-coil3 ) one direction of rotation is working as expected, the other direction the current to the coil is switched off always at the Hall state H1 =L H2=L H3=H. This will stop the motor at slow speed.
Changing the connection of the motor to OUT1-coil2, OUT2-coil3, OUT3-coil1 and the hall sensors accordingly will cure the problem.
Changing the connection to OUT1-coil3, OUT2-coil1, OUT3-coil2 the problem returns but the motor will stop with at the hall state H1=L, H2=H, H3=L.
Looking at the hall signals with an oscilloscope during motion shows a pattern as expected just added with some noise.
We got the problem with the eval board L6235N and also with our own board with the L6235PD.
I bought also an eval board of the L6229 and this IC works without problems!!!!
Can you explain the behavior of the L6235 ? Why is the current to the coil switched off without showing anything on the DIAG Pin ?
Best regards
Georg Spörl
t +49(0)7225 684 – 523
f +49(0)7225 684 – 900
e G.Spoerl@precitec.de<mailto:G.Spoerl@precitec.de>
i www.precitec.de<http://www.precitec.de>;
Precitec GmbH & Co. KG
Draisstraße 1
76571 Gaggenau
Germany
Amtsgericht Mannheim, HRA 521141
Komplementär GmbH/Unlimited Liability Partner: Precitec Consulting GmbH, 65760 Eschborn, Amtsgericht Frankfurt/M, HRB 75364
Geschäftsführung/Managing Board: Dr. Benno Stork gen. Wersborg, Dr. Thilo Stork gen. Wersborg, Dr. Michael Bauer, Dr. Stephan Biermann
******************************************************************************************************************************************
This correspondence was compiled with due diligence, however information (e.g. technical data, delivery times and prices) is provided 'as is'. Precitec cannot guarantee completeness, accuracy or reliability. This message may contain confidential and/or privileged information. If you are not the addressee or authorized to receive this for the addressee, you must not use, copy, disclose or take any action based on this message or any information herein. If you have received this message in error, please advise the sender immediately by reply e-mail and delete this message. Thank you for your cooperation
******************************************************************************************************************************************
Von: Enrico Poli
Gesendet: Mittwoch, 1. Februar 2017 14:33
An: Spoerl Georg
Betreff: Re: - Re: L6235 commutation scheme
STMicroelectronics Community <https://community.st.com/?et=watches.email.thread>
Re: L6235 commutation scheme
reply from Enrico Poli<https://community.st.com/people/Poli.Enrico?et=watches.email.thread> in Power Management and Motor Control - View the full discussion<https://community.st.com/message/145175-re-l6235-commutation-scheme?commentID=145175&et=watches.email.thread#comment-145175>
________________ Attachments : image002.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hyg8&d=%2Fa%2F0X0000000bEQ%2FW8O4Mc04fyXxUr.zVaywQMmFscPwPPUcJfWQTAzWQ5A&asPdf=false_EC13.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hyxh&d=%2Fa%2F0X0000000bES%2FQ3Pi4MnJzP0QP_IYMsvNSHr1TZRDbszFnE6JRzARRfU&asPdf=false