2021-01-27 2:28 AM
According to the data sheet of the LED7708 it is not clear to me how to read the DEVCFG0 register. Since the bits OVFW, OTAF, OCAD, SCAD, contain status messages, I would like to be able to determine the cause of a fault. The firmware of the STEVAL ILL035V1 shows the following example:
//==============================================================================
// This routine sends a 16-bit word to the device
// and returns the rolled out value
//==============================================================================
u16 Write_16(u8 Destination, u16 Data_to_Send)
{
int i;
u16 flag, Mask;
u16 Received_Data=0;
int ReceivedStream[Max_Packet_Lenght];
GPIO_ResetBits(GPIOB, BUSY); // Busy LED on
Mask=0x8000;
Received_Data=0;
for(i=1; i<=16; i++)
{ // number of bits
flag = Data_to_Send&Mask;
if(flag)
{
GPIO_SetBits(GPIOA, SDO); // SDO high
GPIO_SetBits(GPIOA, SCK); // SCK high
if(GPIO_ReadInputDataBit(GPIOA, SDI))
{
Received_Data=Received_Data|Mask;
ReceivedStream[i] = ReceivedStream[i]|Mask;
ReceivedStreamNEW[i] = Received_Data;
}
GPIO_ResetBits(GPIOA, SCK); // SCK low
}
else
{
GPIO_ResetBits(GPIOA, SDO); // SDO low
GPIO_SetBits(GPIOA, SCK); // SCK high
if(GPIO_ReadInputDataBit(GPIOA, SDI))
{
Received_Data=Received_Data|Mask;
ReceivedStream[i] = ReceivedStream[i]|Mask;
ReceivedStreamNEW[i]=Received_Data;
}
GPIO_ResetBits(GPIOA, SCK); // SCK low
}
if(Destination!=0)
{
if (i==(16-Destination))
{
GPIO_SetBits(GPIOA, GPIO_Pin_4); //LE high
}
if (i==16)
{
GPIO_ResetBits(GPIOA, GPIO_Pin_4); //LE low
}
}
Mask=Mask/2;
}
GPIO_SetBits(GPIOB, BUSY); // Busy LED off
return(Received_Data);
}Based on the latch, the operations on the LED driver are distinguished. How is distinguished whether DEVCFG0 or DEVCFG1 is written/read?
2021-02-01 12:14 AM
In the meantime I was able to port the 16x12 bit mode successfully.
The 1x192-bit or 1x256-bit mode, which continuously sends back the status of all registers, unfortunately does not work. There is also no complete example from ST for this mode. Does nobody have any experience with this LED chip?