cancel
Showing results for 
Search instead for 
Did you mean: 

Hi I would like to use external MOSFET with ST's eFuse part STEF01, because of my Bus Voltage is 145V and bus current would be 3Amp. Pls suggest possible solution. Thanks.

_Sansindhu
Associate
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @_Sansindhu​, to the community!

STEF01 can drive an external FET, but it is in series and only serves to protect against polarity reversal. Since the STEF01 is connected to the full input voltage, but is destroyed above 55V, it cannot work with your 145V.

By the way, all our e-fuses currently work up to a maximum of 55V, so we cannot yet recommend a possible solution.

Does it answer your question?

Regards,

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
_Sansindhu
Associate

Thanks Peter!

Your're welcome!

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.