cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I am working on STC3117 for voltage and SoC detection. So far I am able to get voltage correctly but current values and SoC are wrong. Please check configuration if anything wrong.

DGadh
Associate

Configurations are as follow

I am using default OCV table and 660mAh battery (4.2v max) with <70 mOhm internal impedance

first OCV value = 7788

REG_CTRL

vBattTWI_Write(1, BATT_GAUGE_ADD, REG_CTRL, 0x02);

REG_MODE

vBattTWI_Write(1, BATT_GAUGE_ADD, REG_MODE, 0x30);

After configure current value

current = 65533

and

OCV = 7103

Final values while monitor I am getting

I = -1 mA

SoC = 80%

Charge value = 52

#STC3117

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0