2020-06-04 1:50 PM
Does the chip measure time between microsteps to properly compensate BEMF when in voltage mode?
2020-06-10 10:26 AM
The answer is in external step mode, the motor is considered stopped, and no BEMF compensation is used,
so in other words, Voltage mode is almost completely useless when using external step mode, which is a tragedy
because I really needed the smoothness of voltage mode.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.