cancel
Showing results for 
Search instead for 
Did you mean: 

ELECTRONIC CARD DEVELOPEMENT

f_
Associate
Posted on May 14, 2013 at 16:40

I have to develop an electronic card for driving a DC bipolar brush motor for traction use. I need drive it in PWM mode to change RPM and also I need to reverse polarity to change revolutions direction. PWM and directions signals are provided by an 8 bit microcontroller.

The motor parameters are the follow:

Rated Voltage= 12VDC, Rated Power=400W, Rated Speed=2800rpm,

Rated Current=32.9A, Start Peak Current=98.7A, Total Resistance=0.04Ohm,

Inductance=0.08mH, Torque Constant=0.033Nm/A, Voltage Constant=4.0V/K rpm,

Electrical Time Constant=2.0 ms.

Please can you help me with some tips and/or shematics examples, driving methods?

Thank you in advance.

Best Regards
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0