cancel
Showing results for 
Search instead for 
Did you mean: 

Do I need optocoupler to connect Steval-IHM023V3 to the microcontroller?

AKhia
Associate

Hello,

I want to use Steval-ihm023v3 as my motor driver and I am using a TI microcontroller. I have two questions:

  1. Do I need to use opto-couplers to connect PWM pins of the driver to MCU?
  2. Do I need to have signal conditioning fo reading the currrent of the phases? From the schematics, I can see that the voltage of the shunt resistors are passed through Op-amps, but I want to make sure that this voltage is under 3.3V so that it won't ruin the ADC and MCU.

Regards,

Ata

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0