cancel
Showing results for 
Search instead for 
Did you mean: 

Changing the PWM-Frequency at runtime

glubschi_sp
Associate II
Posted on January 12, 2005 at 07:15

Changing the PWM-Frequency at runtime

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
glubschi_sp
Associate II
Posted on May 17, 2011 at 10:18

Hi,

I'm use the St7FMC2N6B6 controller in an inverter. Is it possible to change the PWM-frequency while the motor is running? Have the outputs to be seperated? Or can I change the PWM counter prescaler without stopping the outputs?

Are the corresponding bits in the ARTCSR Register (Bit CC[2..0])?

Best regards,

Micha

gaetano
Associate II
Posted on May 17, 2011 at 10:18

Hi,

it is possible to change the PWM frequency runtime as you are saying. If you open the ST7MC datasheet at page 196 ''PWM Generator Block'' paragraph, you will find how the system works.

Best regards,

Tanio

glubschi_sp
Associate II
Posted on May 17, 2011 at 10:18

Thank you very much for your fast help!

That means, a adaptive PWM-frequency is possible, to reduce powerlosses in the powermodule. Not bad!

Best regards,

Micha