cancel
Showing results for 
Search instead for 
Did you mean: 

Can the high voltage L9907 Driver Circuit be installed?

mustafacmk
Associate II
Posted on July 12, 2018 at 16:39

I want to do a motor drive with the l9907. I have STP315N10F7 Mosfet. But there is a problem. The driver says that it supports up to 54V, but I want to use the MOSFET drain pin with 85V. How can I do that?

#motor-control #motor-driver-ic
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0