cancel
Showing results for 
Search instead for 
Did you mean: 

BLDC Error FOC with ST Motor Control Workbench

tom1
Associate

Greeting!

First of all I'm quite new and not really familiar with the STM products.

I want to control a BLDC motor (Turnigy Multistar 4225-390Kv 16Pole) with the Steval-spin3201.

When I connect the ST MotorControl Workbench with the eval-board and press "start motor" or "user button 1" the status changes from idle to FOC duration.

My approach is listed below:

1) Connect all needed cables

2) Supply voltage setup

3) Connect eval-board with USB-cable to the PC

4) Start MotorControl Workbench

5) Setup moror parameters (poles ...) and choose eval-spin3201 board

6) Lower the PWM frequency to 8000Hz

7) Generate Project (Toolchain: ST SW4 STM32; with HAL)

8) Start System Workbench for STM32

9) Open the projects (STSPIN32F0_MC Library and STSPIN32F0_UserProject)

10) Build All and debug as it is discrebed in the user manual

11) Open Monitor in ST MC WB

12) Connect to the eval-board with the right port and baudrate

-Status is "IDLE"

13) Start Motor

-Status is "FOC duration"

I checked two phases with my oszi and received this kind of signal when I hit the start button. At the moment I'm not sure where the problem is.

Many thanks in advance!

PS: I used the user manual "Getting started with the STSPIN32F0 FOC firmware example

STSW-SPIN3201" UM2152

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0