Question
Adding soft-start to LDL1117
Posted on April 27, 2018 at 04:00
Hi,
I'd like to use the fixed 3.3V variant of the LDL1117 on my board. However, I have a concern with inrush current and wanted to add a soft-start if possible. Can I modify the LDL1117 circuit to add in soft-start (i.e. adding a cap somewhere to control the ramp) or would it be better to add an external inrush limiter such as shown in the following app note:
http://www.ti.com/lit/an/slyt096/slyt096.pdf
?Thanks!
Matt