2025-12-11 4:48 PM - last edited on 2025-12-18 5:34 AM by Amel NASRI
Hello STM Community -
This post is in reference to the recent STM32U3 workshop webinar. I worked through the rather involved / complicated setup associated with the NFC example. Once the code was generated, 23 errors were returned during compilation. Not sure whether to chase down the 23 errors or request a "known good" project ZIP. I really just wanted to see the NFC function with the STM32U3 series MCU's. Pls advise.
Thanks much,
Kelly
2025-12-16 2:48 AM
Hello @Kbitsnbyte ;
Could you please share your project?
If you want to generate code from .ioc file using STM32CubeMX toolchain, I recommend you to copy the .ioc file in a new workspace then generate code and open the project using STM32CubeIDE
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-12-17 8:14 AM
Hello Kaouthar - a few updates:
Thanks much,
Kelly